Case Study

Windsor Park streamlines facilities management with TheWorxHub

A 60-acre continuing care retirement community (CCRC) leveraged TheWorxHub to track equipment history, bill services and give inspectors real-time proof of completed work

Seating area near a lake with a fountain

Windsor Park

Windsor Park has a 60-acre campus in Carol Stream, Illinois, with 7 maintenance staff and 400 apartments.

Brightly Software was acquired by Siemens. All products and services are now offered under the Siemens Asset Management portfolio.

https://www.covlivingwindsorpark.org/

Headquarters
Carol Stream, Illinois, USA
Products
Industry Sector
Senior Living
Additional cost savings exist around asset management and knowing, based on the tracking of your work on a particular piece of equipment, where you fall within the repair versus replace decision.
Bob Lanzerotti
Facilities Management Director, Windsor Park

Background

Bob Lanzerotti is the Facilities Management Director at Windsor Park, which is a CCRC catering to the needs of a variety of residents with a wide range of needs, from independent living to skilled care.

“Our previous system was not user friendly, involved a lot of paper and the reports were not what we were looking for. There was a lack of communication, and it was not uncommon to lose track of work orders. It was old and antiquated. Because of the diversity of our campus, we needed a better system in place,” Lanzerotti says.

“With TheWorxHub, one of the biggest advantages is the ability to track the history on a piece of equipment,” continues Lanzerotti. “Recently we’ve experienced turnover in one of our positions and have a new employee. It was easy for him to go into the system and pull up all the historical work orders for the two buildings he’s responsible for. This allows him to see a history of work on any piece of equipment to determine a path of action based on real data. During times when we’ve needed to hire an outside contractor, it’s simple to pull a report that includes PMs that need to happen on 15, 20 different pieces of equipment. Then, you just hand it over to them and they love it.”

Improving resident service with efficiency

Going back to the diversity of its residents, Lanzerotti says Windsor Park can be asked to perform a variety of “extra” tasks. “With paper, it can be very difficult to keep track of and bill for,” he says. “For instance, we have an IT person starting who will be available to assist our residents with their individual IT needs, and, because we’ll be able to properly track the work, we will be able to incur additional income from those tasks. Our accounting department will be able to very easily view those charges and bill individuals accordingly. On a monthly basis, we are probably billing an additional 15–20 jobs.

“Also, with $4.5 million spent a year on refurbishments, we can track the work that’s needed, how often it needs to occur, as well as all of the actual assets that are added to our buildings.

“As far as ease of use, a perfect example is when the state inspector visited last month, she pointed out something that we were going to be tagged for. We were able to pull up the work order history, do the work, take a picture and show it to her completed prior to her leaving our campus. We utilize the photo capabilities almost daily.

“I would suggest when looking for a system to make sure it’s user friendly. You can have the most complicated, supposedly the best, but if you don’t know how to use it to be able to get the value, then why have it?”

With $4.5 million spent a year on refurbishments, we can track the work that’s needed, how often it needs to occur, as well as all of the actual assets that are added to our buildings.
Bob Lanzerotti
Facilities Management Director, Windsor Park

Get Quarterly Insights